View the status of the axis
Use the
Status
page in the Axis Properties
dialog box to display the current status of the axis and digital I/O.
TIP:
The available parameters depend on the
Axis Configuration
on the General page
.Before you begin:
- The device must be online to view the status information.
To view the status of the axis:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickStatus.
- TheAxis Statusshows the status of the axis. The LED next to each axis state lights up when it reaches that state. If the limit is not reached, the LED remains gray.
- TheDigital I/Oshows the state of the I/O. The LED next to each digital I/O state lights up when it reaches that state.
Provide Feedback