Unable to modify source protection for the following component(s)

This table describes error conditions that can prevent changes to component source protection.
Error condition
Possible solution
  • The license or source key is not available.
  • Do not have the required permission.
Insert a
CmStick
with the required license with
Protect
permission, or add the source key to the sk.dat file for the component(s).
The Add-On Instruction is sealed.
Unseal the Add-On Instruction, apply source protection, and re-seal it.
The
Viewable
option for the component was not selected or unselected.
When attempting to set or clear the
Viewable
option, only select source-protected components for which the source key is available.
License Source Protection is not supported for Sequential Function Chart (SFC) or Function Block Diagram (FBD) routines.
None.
License Source Protection is not supported on safety components on
Compact GuardLogix
5380 and
GuardLogix
5580 controllers
.
None.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.