deviceCategory
Defines the device type, such as a controller.
[deviceCategory] <controllerType/deviceType> [name] { <property name> := <property value>; ... <timeSync> <ports> ... <physicalPorts> ... <tags> ... }
This table lists the type elements.
Element | Description |
---|---|
type (required) | Device type. |
controllerType/deviceType | Defines the type of controller or device. Must match a controller or device catalog number, such as name=_1756_L85E. |
name (required) | Name of the device. |
minorRev | Current minor revision of the device. |
catalogNumber | Device catalog number. |
desc | A brief description of the device. |
privateData | Defines all data needed for use by the AOP and controller profiles. Important: Do not modify this content. Changing this content can prevent the device profile from opening, and the device will have to be deleted and re-created. |
portMode | Current configured port mode. For devices that support this element, it defines the physical ports as linear or dual port mode. |
redundancy | Indicates that the device supports redundancy. |
inhibited | Indicates that the user has inhibited this device. |
moduleEKeyingState | Type of electronic keying configured: Disabled, CompatibleModule, or ExactMatch. |
Provide Feedback