DriveOvervoltageFault

Applies to: Servo Drive axes.
DriveOvervoltageFault is a Boolean attribute. It is set when drive DC bus voltage exceeds the predefined operating limits for the bus.
DriveOvervoltageFault is a recoverable fault.
To clear a DriveOvervoltageFault:
  1. Check or increase the drive’s regenerative load capacity.
  2. Change the load profile.
  3. Be sure your program or fault handling routine contains a Fault Reset (MAFR) instruction, to clear all motion faults for an axis.
The occurrence of a DriveOvervoltageFault sets bit #24 of the DriveFault attribute, the PhysicalAxisFault attribute and bit #0 of the AxisFault attribute.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.