By Bill (Buff) Crosley, systems product manager and Mark Indgjer, applications engineer, Flame & Gas Safety Systems, Det-Tronics
Editor's Note: This article is adapted from a comprehensive white paper, "Integrating Fire and Gas Safety with Process Control Systems: Why, What and How." Download the free, full white paper with additional information about guidelines from standards organizations, regulatory bodies and industry groups; why fire and gas (F&G) safety systems are needed; and subsystems in a F&G safety system, including flame, gas and smoke detection, the safety system controller, and notification and suppression-activation devices.
If a fire or gas leak is detected in an industrial facility, prescriptive actions must be taken by the fire and gas safety system and the process control system to mitigate and control the hazard. Using a certified, documented fire and gas safety system that can communicate appropriate messages to the process control system during an event is vital to worker and facility safety. However, specifying and integrating these two systems is no simple matter.
Mitigating a Hazardous Event that Has Already Occurred
Under certain conditions, processes in industrial, high-hazard manufacturing or processing plants can threaten the safety of employees, operations and the environment. In these settings, a fire and gas (F&G) safety system is the layer of protection responsible for mitigating consequences of a hazardous event once it has occurred.
Consider a chemical plant where flammable materials continue to be pumped into an area where fire has been detected. In hazardous situations like this, it’s imperative that an F&G safety system communicate with the process control system (PCS). The relationship between a plant’s F&G safety system and the operation’s PCS is prescribed by multiple standards.
Here’s a simple overview of what makes up process control and safety systems.
Process Control
- Process Control System (PCS)
- Process Instrumentation
Safety
- Process Shutdown System (PSD)
- Emergency Shutdown System (ESD)
- Fire & Gas Safety System (F&G)
- Flame, Gas and Smoke Detection
- Safety System Controller
- Notification and Suppression/Activation
In the United States, National Fire Protection Association standard NFPA 72® National Fire Alarm and Signaling Code® dictates that the F&G safety system can’t be interrupted by the PCS.