Instrument Maintenance Management
Modern instrumentation provides status and diagnostic information, but processing all of this data is often a problem. For example, at Thomas’ chemical plant in Germany, having its control systems read all the diagnostic information from all 4,000 devices, analyze it for problems, and issue instructions to the maintenance department would be a daunting problem for the plant’s control system programmers. It would also burden the control system with data not relevant to its primary task, which is real-time process control.
Instead, instrument manufacturers have developed software packages that perform all those functions. The packages fall into two basic categories: 1) instrument management programs, which analyze real-time information from instrumentation; and 2) asset management software, which keeps track of every instrument in the plant and stores vital data, such as manuals and parts lists.
Instrument management programs perform several functions to help maintenance departments, including:
- Configuration: helps maintenance configure new instrumentation during initial installation or when replacing an existing instrument.
- Condition monitoring: used to analyze real-time data coming from instrumentation, look for problems, and notify the maintenance department when a device needs attention prior to failure.
- Life-cycle management: tracks the entire life cycle of an instrument, from initial configuration to calibrations and repairs, and provides information for audits and safety regulations.
While a particular instrument manufacturer can provide information for its own instruments, what about all the other instruments in a plant from different manufacturers? Fortunately, standardization across the instrumentation industry makes that information available.
Endress+Hauser, a global provider of process measurement instrumentation, services and solutions, is a Strategic Alliance Partner in the Rockwell Automation PartnerNetworkTM program. Together, Rockwell Automation and Endress+Hauser deliver integrated pre-engineered, pre-tested, supported, and maintained instrumentation and control and information solutions that provide plant-wide advanced diagnostics and process system life-cycle management.
The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Putman Media, Inc.