Mobile terminal allows operators to make real-time changes to out-of-view applications
MILWAUKEE, June 8, 2015 — Rockwell Automation has introduced its new Allen‑Bradley MobileView tethered operator interface. The mobile terminal gives plant and industrial personnel the freedom to take a machine’s human-machine interface (HMI) with them to make real-time adjustments to out-of-view applications.
The MobileView tethered operator interface is ideal for maintenance tasks, machine setup or calibration activities, and other HMI applications that require the operator to see the machine. The inclusion of a hardwired e-stop button and three-position enabling switch also supports applications that require local safety functionality.
“Between making an adjustment on the terminal and viewing the results on the machine, fixed operator terminals can require a lot of back and forth for personnel, for certain applications,” said Matt Hansen, senior product manager at Rockwell Automation. “The MobileView tethered operator interface puts the terminal in the operator’s hands to increase productivity and safety. Tasks are made more efficient and machines are set up faster.”
The MobileView tethered operator interface complements the Allen-Bradley PanelView graphic terminals, giving manufacturers and industrial operators a range of fixed and mobile terminals for different applications. It also uses the FactoryTalk View Machine Edition (ME) HMI software from Rockwell Automation, allowing users to develop and re-use their software applications across the MobileView and PanelView platforms.
Three cable-length options, ranging from 16.4 feet to 49.2 feet, offer flexibility for different machines and production lines. The MobileView tethered operator interface also uses a 10-inch display with resistive touch screen, 2 GB internal SD card for application storage, and USB 2.0 port for high-speed data transfer. Software assignable functions are available as an option with either a hardwired momentary illuminated pushbutton or three-position key switch.
News Release Assets
Image available upon request or here at box.com.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,500 people serving customers in more than 80 countries.
Media Contacts
Tiffany Pfremmer
Rockwell Automation
414.839.7425
tbockhop@ra.rockwell.com
Leanne Hanson
PadillaCRT
612.455.1776
leanne.hanson@padillacrt.com
Allen-Bradley, FactoryTalk, LISTEN. THINK. SOLVE., MobileView and PanelView are trademarks of Rockwell Automation Inc.
Published June 7, 2015