Develop an interface for switching locales

Create a localized label and two buttons that change the interface language.
Application example - English locale
Application example - Polish locale
NOTE:
Download a sample project:
ExampleApplication-SwitchLocales.zip
Prerequisites
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
Application design example
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.