Develop an interface for interacting with a database

Develop NetLogics that: insert values into the database, query the database, and display the query results.
Application example
TIP:
You can download a sample project from:
ExampleApplication-InteractWithDatabase.zip
Prerequisites
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.