- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Define methods in C#
You can define methods and OPC UA methods in C#.
Method
Within a NetLogic, you can define a new method (for example,
Foo
) by using the following syntax:
public void Foo() { // Code to run }
TIP:
You can define multiple methods within a class.
OPC UA method
OPC UA methods:
- Can be referenced inFactoryTalk Optix Studioat design time.
- Are callable at runtime.
To define an OPC UA method, add
[ExportMethod]
before the method. See the following example.
[ExportMethod]public void Foo() { // Code to run }
TIP:
You can create an OPC UA method by using
FactoryTalk Optix Studio
. See Create an OPC UA method.Method arguments
You define method arguments in round brackets
()
after the method name.An OPC UA method can have any number of input and output arguments.
IMPORTANT:
If you edit the arguments of a method associated with an event in
FactoryTalk Optix Studio
, you must re-associate the method.To define an input argument:
- Indicate the data type between the round brackets followed by the argument name.
- Separate each argument with a comma.
In the following example, two integer input arguments,
speed
and rpm
, are declared:
public void Foo(int speed,int rpm) { // Code to run }
To define an output argument:
- Indicate the keywordoutfollowed by the data type and argument name between the round brackets.
- Separate each argument with a comma.
- Assign the values to the output arguments.
In the following example, two output arguments are defined,
result
and motorSpeed
, of string and integer types respectively:
public void Foo(out string result,out int motorSpeed) { result= "Ok"; motorSpeed = motor.speed; }
You can define both input and output arguments for the same method. In the following example, two input and two output arguments are defined:
public void Foo(int speed,int rpm,out string result,out int motorSpeed) { result = "Ok"; motorSpeed = motor.speed; }
Provide Feedback