Projects
A
FactoryTalk Optix Studio
project contains different components that you use to create FactoryTalk Optix Applications
.A project can include these elements:
- Objects. Physical objects such as a motor or non-physical objects such as a digital alarm.
- Object types. Model objects from which you can create object instances. Each object instance can contain specific objects and variables.
- Variables. Elements that represent characteristics of objects and specify the values of these characteristics.
- Variable types. Model variables from which you can create variable instances, which can contain other specific variables.
- Runtime method types. Model methods from which you can create method instances. Method instances can execute at runtime when an event, such as a user action or a change in a variable value, occurs.
- Graphic objects library. A predefined library of objects, such as controls, containers, drawings, or media content, that you can use to create a user interface forFactoryTalk Optix Applications.
- NetLogic. NetLogic objects that implement custom application logics developed in C#.
Provide Feedback