Edit a template
Edit a template to change the attributes of objects and variables that you create that are based on the template.
- On your computer, navigate to the folder.C:\Users\UserName\Documents\Rockwell Automation\FactoryTalk Optix\Libraries
- Expand the folder of the desired library.
- Open the project that has the same name as the library.
- SelectTemplateLibraries.
- Open the desired library folder.
- Add and remove templates in the library.
- Edit the objects that are in the library. InProjectview, select the object and then edit the variable values inProperties.
Provide Feedback