Develop buttons for closing and shutting down

Develop buttons for closing and shutting down

Create buttons that close the
FactoryTalk Optix Application
and shut down the host system.
IMPORTANT:
Pressing
Shut down system
immediately shuts down the host operating system
on which the
FactoryTalk Optix Application
runs.
For example, if you run the
FactoryTalk Optix Application
on an emulator target, pressing
Shut down system
immediately shuts down your Windows system.
Application example
TIP:
Download a sample project:
CloseApplicationShutDownSystem.zip
Prerequisites
Application design example
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.