- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Constructor: PeriodicTask(action, periodMilliseconds, excutingNode)
A
PeriodicTask
task runs code at regular time intervals.PeriodicTask(Action action, int periodMilliseconds, IUANode executingNode);
Arguments
- action(Action)
- The method or lambda expression to run.
- periodMilliseconds(int)
- The time between the method or lambda expression runs.
- executingNode(IUANode)
- The node in which the code runs.
Example
The
myPeriodicTask
task runs the IncrementVariable()
method every second (1000 milliseconds). The method increments the value of the variable1
variable by one unit each time it runs.
public override void Start() { myPeriodicTask = new PeriodicTask(IncrementVariable, 1000, LogicObject); myPeriodicTask.Start(); } public override void Stop() { myPeriodicTask.Dispose(); } private void IncrementVariable() { variable1.Value = variable1.Value + 1; } private PeriodicTask myPeriodicTask;
TIP:
In this example, the
IncrementVariable()
method has no PeriodicTask
argument because the simplicity of its code does not require the task to be canceled.Provide Feedback