Configure a local library

Configure a custom local library to store templates of objects and variables.
TIP: To use a custom local library on another computer, copy the folder with the library name from
C:\Users\
UserName
\Documents\Rockwell Automation\FactoryTalk Optix\Libraries
to the same location on another computer. Alternatively, you can use remote libraries. See Configure a remote library.
  1. From the main toolbar, select
    Template Libraries
    .
  2. In
    Template Libraries
    , select
    Add
    and select
    New library
    .
  3. (optional) Enter a name for the library.
    TIP: In order to use version control, FactoryTalk Optix library names and repository names must match. The library and repository names must contain only alpha numeric characters, numerals, periods, dashes, and underscores.
New library appears in
Template Libraries
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.