Export nodes to NodeSet

Export nodes to a NodeSet
XML
file. Use the exported file to exchange
OPC UA Companion Specifications
.
Prerequisites
Add nodes to the project. See Project nodes.
  1. To export nodes to NodeSet
  2. In
    Project view
    , right-click a node to export and select
    Export to NodeSet
    .
    TIP: You cannot export the root project node.
  3. Select a location for the NodeSet
    XML
    file.
    The selected node and child nodes are exported.
  4. (optional) In the export notification, select
    Open containing folder
    to navigate to the exported NodeSet
    XML
    file.
Import the NodeSet to an OPC UA server, another
FactoryTalk Optix
project, or browse the nodes offline in an OPC UA client.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.