Configure OPC UA client certificates and keys

Edit the properties of an OPC UA client object to configure the public certificates and private keys.
Prerequisites
  1. In
    Project view
    , select an
    OPCUAClient
    object.
  2. In
    Properties
    , next to
    Client certificate file
    , select
    Browse
    .
  3. In :
    • If the certificate is listed, select the certificate and choose
      Select
      .
    • If the certificate is not listed:
      1. Select
        Import file(s)
        .
      2. Select the certificate. For more information, see Certificates and keys location.
      3. Choose
        Select
        .
  4. In
    Properties
    , next to
    Client private key
    , select
    Browse
    .
  5. In :
    • If the private key is listed, select the private key and choose
      Select
      .
    • If the private key is not listed:
      1. Select
        Import file(s)
        .
      2. Select the private key. For more information, see Certificates and keys location.
      3. Choose
        Select
        .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.