Duplicate a recipe schema
Duplicate an existing recipe schema to base the new schema on the old schema.
- From the toolbar, select.Open dashboard page
- In the central pane, selectConfigure a recipe.
- Right-click the available recipe schema and selectDuplicate.
If necessary, edit the duplicated recipe schema. See Edit a recipe schema.
duplicate
Provide Feedback