Create a button to restart the application

You must restart the
FTOptixApplication
to have date and time changes from the widget take effect.
Create a button to restart the
FTOptixApplication
.
  1. In
    Project view
    , right-click the folder to contain the button and select
    New
    Base controls
    Button
    .
    Button# (type)
    appears in
    Project view
    .
  2. With
    Button# (type)
    selected
    , in
    Properties
    under
    Events
    , select
    Add
    Add new method
    next to the event, such as a
    MouseClick event
    , that you want to restart the
    FTOptixApplication
    .
  3. Expand
    Core commands
    , select
    Restart
    , and then choose
    Select
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.