Network ports configuration

Network ports configuration

Configure firewalls and ports to ensure successful communication. Review the default values for user-configurable ports and the comprehensive list of ports used by
FactoryTalk Optix
for inbound and outbound connections.
TIP: Ports 80 and 443 may be already configured for devices like OptixPanels and Embedded Edge Compute Module (EECM).

FactoryTalk Optix modules

  • WebPresentationEngine
    • Protocol: This port is configurable. If Protocol is blank, the port reflects the protocol configuration.
      • If set to HTTP: 80/TCP
      • If set to HTTPS: 443/TCP
  • ApplicationUpdateServer
    • Fixed Port: 49100/TCP
  • Communication Drivers
    • RA Ethernet/IP Driver
      • Port: 44818/TCP
    • Modbus
      • Port: 502/TCP
    • Melsec FX3U: Configure the TCP port on PLC.
      • Default port: 1034/TCP
    • Melsec Q: Configure the TCP port on PLC.
      • Default port: 1/TCP
    • Omron Ethernet/IP
      • Port: 44818/TCP
    • Omron FINS
      • Port: 9600/TCP
    • S7 TCP
      • Port: 102/TCP
    • S7 TIA
      • Port: 102/TCP
    • TwinCAT
      • Port: 851/TCP
    • CODESYS
      • Port: 1217/TCP
  • DataStores
    • SQL/SQL Express
      • Port: 1433
    • MySQL
      • Port: 3306
  • User Authentication
    • LDAP: Configurable in the domain server address
      • Default port 39.
    • AD: This port is configurable. If AD is blank, the port reflects the protocol configuration.
      • The default port is 39.
  • OPC UA
    • Server: User-configurable
      • Default port: 59100/TCP
    • Client
      • The port depends on source server configuration.
  • FTRA Service
    • Ports: 5000/TCP, 14273/TCP, and 5936/TCP
  • FT Hub
    • FactoryTalk Optix acts as a client, using a random port at every connection.

External modules from TemplateLibrary

  • MQTT (PushAgent and MQTTLogic):
    Configure these ports depending on the server configuration:
    • Standard: 1883/TCP
    • Secure: 8883/TCP
  • Email (AlarmsWithEmailNotification):
    Configure these ports depending on the server configuration:
    • SMTP
      • 57/TCP, 25/TCP, or 465/TCP
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal