Activate a Runtime entitlement on Windows devices

Activate a Runtime Tools entitlement to launch the application on the Runtime device.
  1. Select the Windows
    Start
    menu and start typing
    Entitlement Manager
    or double-click the FactoryTalk Optix studio icon on your desktop.
  2. In
    Entitlement Manager
    , under
    Installed entitlements
    , select the entitlement type:
    • Online
      : Activate an online entitlement.
    • Offline
      : Activate an offline entitlement.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.