Runtime as a service

FactoryTalk Optix
runs the deployed application as a Windows service. You can optionally interact with the application using the web browser of any device that can access the Runtime device through an Ethernet IP address. The application starts when Windows opens, without the need for a user to sign in.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.