Configure the IP Address, BOOTP Setting, Port Speed, and Duplex (SoftLogix5800 EtherNet/IP Module)
To configure the IP address, BOOTP/DHCP settings for this module, you must use the configuration tools provided for it on your desktop. This module cannot be configured using the
Logix Designer
configuration application.The fields on the Port Configuration tab of the Module Properties screen for this module are for informational purposes and are therefore read-only. You will not be able to make modifications to these properties.
Accessing the Module Properties dialog - Port Configuration tab
To access the Port Configuration tab of the Module Properties dialog, right click the appropriate module from the Controller Organizer, and choose Properties. The Module Properties dialog appears, with the General tab selected. Click the Port Configuration tab.
Provide Feedback