Load Share Tab
Use this tab to enter the load share settings.
Parameters
Full Scale Voltage
This is the value the load share output will reach when the generator is producing 1 p.u. kW. The base for this calculation is the calculated generator kVA. Valid values range from 0 to 4.0 V (default).
Limit
This is the value for the amount of per unit change allowed in the load share output per unit of time. Valid values range from 0 to 1.0 P.U.; the default value is 0.3 P.U..
Rate
This is the value for the time required for the load share output to change the per unit amount. Valid values range from 0 to 100.0 sec/Rated Watts; the default value is 10.0 sec/Rated Watts.
OK
Click this button to accept your edits on any tab and close the dialog.
Cancel
Click this button to cancel your edits on any tab and close the dialog.
Apply
Click this button to apply your edits on any tab and continue editing.
Help
Click this button for help on this tab.
Provide Feedback