Limits page
Use the settings on the
Limits
page to configure limits manual tuning parameters. Use the page to:- Enter the positive and negative peak torque limits.
- Enter the acceleration and deceleration limits.
- Enter the positive and negative velocity limits.
TIP:
To open the Limits page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- In the lower left of theAxis Propertiesdialog box, selectManual Tune.
- In theMotion Consoledialog box, selectAdditional Tune > Limits.
The parameters appear dimmed if the current configuration does not support the parameter and when the axis is not Servo On.
Parameter | Description |
---|---|
Peak Torque Limit Positive | Select a value to limit the positive peak torque to a value in the range of 0 - 1000. |
Peak Torque Limit Negative | Select a value to limit the negative peak torque to a value in the range of -1000 - 0. |
Acceleration Limit | Select a value for a acceleration limit. The values are in the range of 0 - Max Float. |
Deceleration Limit | Select a value for the deceleration limit. The values are in the range of 0 - Max Float. |
Velocity Limit Positive | Select a value to limit the positive velocity. The values are in the range of 0 - Max Float. |
Velocity Limit Negative | Select a value to limit the negative velocity. The values are in the range of 0 - Max Float. |
Provide Feedback