- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Routine Properties dialog box - General tab - Sequential Function Chart Routine parameters
The
General
tab on the Routine Properties
dialog box lists the properties associated with the selected sequential function chart routine. This table describes the parameters on the General
tab.Parameter | Description |
Name | The routine name, which must follow the Logix Designer application IEC-61131 Name Standard. |
Description | A description for the routine that contains a maximum of 512 characters. |
Type | The language type of the main logic in the routine: Ladder, Function Block Diagram, Sequential Function Chart, or Structured Text. |
In Program | The program to which the routine belongs. |
Number of steps | The number of steps in the routine. |
Permission Set | Applies a set of permissions that controls access based on the permissions configured in FactoryTalk Security. The default setting, <Controller Inherited> , applies the same security settings that have been applied to the controller or project. |
Provide Feedback