- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Unlock command
Select the Unlock command to unlock a locked routine or Add-On Instruction. When locked, an authorized user must unlock the routine or Add-On Instruction before viewing or editing.
TIP:
To lock or unlock a component, the source license must be present on a dongle plugged into the computer running the Logix Designer application, and the license must contain the View permission.
Provide Feedback