From Kepware Technologies
The Industrial Internet of Things (IIoT) has introduced unprecedented connectivity and major shifts in the way businesses innovate and operate. To realize the full promise of IIoT, we must all acknowledge the possible peril connected technology presents and each take responsibility for securing the IIoT landscape. We must work together.
With the advent of physical and digital convergence, now that bits and bytes meet flesh and blood, this new world requires a fusion of once disparate disciplines — and even innovation.
Changing Threat Landscape
1. Predators. Software is not new to safety-critical environments, but the growing levels of remote connectivity are changing our threat models — significantly. Systems that once enjoyed air gaps now are deliberately connecting and exposing themselves to myriad accidents and adversaries. Systems that enjoyed relative obscurity from predators now find themselves both prone and prey.
Worse, many of these attacks are being perpetrated by top predators such as nation-state adversaries, with significant resources and tenacity. And perhaps even worse than that, malicious intent is not a prerequisite to harm.
Safety-critical and industrial IIoT environments simultaneously:
- Face some of our most capable and funded adversaries.
- Carry relatively higher consequences of failure.
- Can be significantly under-resourced and immature with regard to cyber hygiene.
2. Ourselves. Most industrial and safety-critical environments are change-averse and far from nimble. As W. Edwards Deming said, “It is not necessary to change. Survival is not mandatory.” But we choose not only survival, but the transformation of the way we innovate and operate. Therefore, we need to act now to fight the inertia that prevents change.
Failing to act, whether willfully or unknowingly, imperils the promise of IIoT, as illustrated in the table.
3. The Relay Race. We are in a complex relay race against the clock, which is perhaps our greatest challenge. The pace of connectivity continues to accelerate and our adversaries’ sophistication is evolving rapidly. But today, the ecosystem and supply chain players are notoriously slow to deploy, change or patch/update.