By Troy Hoffman, business development lead for Safety Services and Nuala Mullan, business development lead for Safety Services, Rockwell Automation
With the increased demand on our industrial workforce, many facilities are expanding the “do more with less” approach when it comes to machine safety.
Engineering, Health and Safety (EHS) and similar professionals are more likely to have their responsibilities expanded beyond programs such as lockout/tagout (LOTO) and Confined Space. They now include knowledge, design and testing of functional safety devices such as light curtains, area scanners and guard gates that historically were the responsibility of the plant engineer or equipment manufacturer.
Although these alternative protective measures (APMs) can complement LOTO when removal of hazardous energy is required for interaction with the machine, there is still a great amount of confusion on the application of each. When do we use LOTO, and when do we use APMs?
The regulation allows for alternative methodologies to be used as long as they’re “as effective as lockout/tagout” for the particular task. And that’s where many companies run into problems.