Rockwell Automation and McRae Integration collaborated to develop FactoryTalk Brew solution for large brewers
MILWAUKEE — Brewing companies that want to succeed in today’s crowded market need to manage risk, maintain quality, drive out costs and reduce inefficiencies in their operations. The new FactoryTalk Brew solution from Rockwell Automation can help breweries manage these challenges and gain a competitive edge.
The FactoryTalk Brew solution is based on the PlantPAx distributed control system from Rockwell Automation. It enables large brewers to standardize and fully automate production, gain an information platform for reporting and recipe management, and tie together information from the automation layer to the MES layer. It can also integrate enterprise-level automation and information to enable The Connected Enterprise and help inform business decisions. The new offering provides a solution to brewers that struggled to build a software layer on their automation platform or had to build an automation platform from scratch.
During production, operators can access the solution from any device and can pull data with reporting parameters already in place. This enables operators to quickly respond to any process or batch issues that may occur – which is critical for larger brewers that have little room for error.
Click to download image.
“The FactoryTalk Brew solution builds on the custom solutions that Rockwell Automation has designed for the brewing industry for over a decade,” said Dave Sharpe, global industry director for Rockwell Automation. “In collaboration with McRae Integration, we leveraged our existing modern DCS platform to deliver a solution for the specific needs of the brewing industry.”
The brewing solution uses a web application to configure automation sequencing and define reporting parameters to help reduce complexity during startup and brewery operation. During startup, the solution can be adapted to the setup of any brewery, with varying tank, tun
“The limited brewery control offerings available in the market meant that we previously had to develop customized solutions for breweries,” said Andrew Bentley, president for McRae Integration Ltd., a Rockwell Automation Solution Partner and member of the Rockwell Automation PartnerNetwork program. “The FactoryTalk Brew solution allows us to deliver enterprise-ready, standardized control with quick access to production-critical information. This will help us provide more value to customers and help them get their brews to market faster.”
The globally supported brewery solution is delivered by Rockwell Automation and certified partner system integrators or OEMs with knowledge of required products and large brewing processes. It is a result of the continued collaboration in the brewing industry between Rockwell Automation and McRae Integration and complements the existing FactoryTalk Craft Brew solution from Rockwell Automation for craft brewers.
About the Rockwell Automation PartnerNetwork Program
The Rockwell Automation PartnerNetwork program offers global manufacturers access to a collaborative network of companies mutually focused on developing, implementing and supporting best-in-breed solutions to achieve plant-wide optimization, improve machine performance and meet sustainability objectives.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.
Media Contacts
Andrea Huter
Rockwell Automation
216.965.3830
ahuter@ra.rockwell.com
Beatrice Zvosec
Padilla
612.455.1914
beatrice.zvosec@padillaco.com
FactoryTalk, FactoryTalk Brew, PartnerNetwork
Published June 11, 2018