Data type member attributes
This table describes data type member elements.
Attribute | Description |
---|---|
Name | The name of the member. |
Datatype | The data type of the member. Can be atomic, structure, or an array. |
Modifiers | (Optional) Hidden; default is visible. |
HostMemberName | Name of the member providing the bit storage for this member. |
BitNumber | Bit position in the host member. |
Provide Feedback