Configure multiple devices
When you add multiple devices at the same time, you can configure basic settings for the devices all at once.
To configure multiple devices
:
- InDevicesexplorer, selectHamburger Menu, then selectAdd device. TheAdd devicedialog box opens.
- Select each catalog number to add to the project. The selected devices appear in theDevices to Addlist on the right of the dialog.
- SelectContinue. TheBulk Configuredialog opens.
- Configure basic properties for each device to add it to the project. The basic properties vary depending on the device type.
- Device name. Enter a unique name for the device.
- Chassis size. Select the number of slots in the chassis.
- Slot number. Select a slot for the device.
- IP address. Enter an IP address for the device.
- SelectFinish. When the devices are added to the project, they are listed in theDevicesexplorer.
Provide Feedback