Alarm Details view
You can open
Alarm Details
view from Alarm Summary
or Alarm Manager
to display detailed information about a selected alarm.Alarm variable | Description |
---|---|
Current state | Current state for Alarm Summary. The Current state field displays value depending on the alarm logic. |
Message | Message associated with the alarm event, which displays when the alarm is active. Displays the message for the highest alarm state applicable. |
Status | Status displays a combination of all the conditions of an alarm. If any condition in the alarm is In Alarm or Unacknowledged, the alarm appears as In Alarm or Unacknowledged. |
Severity | The numeric value mapped to the assigned priority of the alarm condition.
1-250 (Low) 251-500 (Medium) 501-750 (High) 751-1000 (Urgent) |
Confirmed | Displays if the alarm is confirmed. |
Unconfirmed | Displays if the alarm is unconfirmed. |
Inhibit state | When an alarm has more than one inhibit state, the icon of the highest inhibit state appears in the table. If no icon appears, the alarm has good quality, and is not disabled, suppressed, or shelved. |
Name | Name of the alarm object that generated the alarm event. |
Source variable | Variable monitored by the event. |
Quality | Displays information of a fault in case of faulted alarms.
Good - alarm is not in faulted state Bad - alarm is in faulted state: controller cannot be reached or InFaulted variable for IBA/TBA is set to true. |
Event time | The date and time the alarm event occurred. |
In alarm time | The time the selected alarm entered the In Alarm state. |
Out of alarm time | The time the selected alarm entered the Normal or Out of Alarm state |
Shelve duration | The default time for which the selected alarm condition is shelved to prevent the notification of new state changes. Shelve duration is assigned to the alarm in the project |
Max Time Shelved | The maximum time the alarm can be shelved. |
Shelve Time | The time the selected alarm was shelved. |
Unshelve Time | The time the selected alarm was unshelved. If the alarm is currently shelved, this is the time the alarm is unshelved automatically when the shelve duration expires. |
Enable time | The time the selected alarm was enabled |
Disable time | The time the selected alarm was disabled. |
Suppress time | The time the selected alarm was suppressed |
Unsuppress time | The time the selected alarm was unsuppressed. |
Provide Feedback