Create Alarm manager and Alarm summary
Create an
alarm manager
and alarm summary
widgets, to display essential information about alarms in the project.- In the main toolbar, selectTemplate Libraries.Template Libraries
- InTemplate Libraries, selectWidgets.
- UnderComponents, dragAlarm Widgetsto a folder in theUIfolder.AlarmSummary# (type)andAlarmManager# (type)appear in the folder.
- InTemplate Libraries, selectClose.
- (optional) On the editor, configure the properties of the two widgets.
Provide Feedback