CODESYS Driver
Observe these guidelines when working with CODESYS driver.
Controller tags import
You can import tags in these modes:
- Online mode
- Use online mode to import tags directly from the controller at design time or runtime.
- Offline mode
- For more information, refer to the product documentation.
This communication driver supports importing custom data types defined in the controller project in the offline mode.
Provide Feedback