Parent node format

If a dynamic link is set between two nodes of the same data type, you can set the format for the parent node.
Data types of the source node used to set the parent node format include:
Source node data type
Parent node format
Description
Example
  • Int16
  • Int32
  • Int64
  • Integer
  • UInt16
  • UInt32
  • UInt64
  • UInteger
0 (1234)
Decimal representation, without the thousands separator
7.989
7989
Hexadecimal (ff)
Hexadecimal representation
45
2d
Octal
Octal representation
80
55
Binary
Binary representation
45
10010110
FloatDouble
0,# (1234,5)
Rounding to the first decimal place
  • 59,78
    59,8
  • 59,2
    59,2
  • 3152,9
    3.152,9
0,## (1234,56)
Rounding to the second decimal place
  • 45,33994
    45,34
  • 1,8
    1,8
  • 1245,68
    1.245,68
0,### (1234,56)
Rounding to three decimal places
  • 4,5779
    4,578
  • 3,14
    3,14
  • 1528,65
    1.528,65
0.0 (1234.0)
Representation with exactly one decimal place
  • 5,68
    5,7
  • 5,1
    5,1
  • 9597,77
    9.597
0.00 (1234.00)
Representation with exactly two decimal places
  • 5,3
    5,30
  • 10,65
    10,65
  • 5789,564
    5.789,56
0.000 (1234.000)
Representation with exactly three decimal places
  • 70,4
    70,400
  • 87,7897
    87,790
  • 31529,7879
    31.529,788
DateTime
hh:mm
Date/time format, t
05:30
dd/MM/yy
Date/Time format, d
01/05/19
hh:mm:ss
Extended date time format, T
06:01:58
d MMM yyyy
Extended date, format D
1 gen 2019
dd/MM/yy, hh:mm
Extended date/time, format g
01/07/2016, 12:59
d MMM yyyy, hh:mm:ss
General date/time layout, format F
1 feb 2019, 6:15:28
yyyy-MM-ddThh:mm:ss.0000000Z
ISO 8601 Standard, format o or O
2019-01-07T00:00:00.0000000Z
Duration
[d.]hh:mm:ss[.0000000]
Format c
2.09:10:2006:10:20
[d:]h:mm:ss[,0000000]
General short format, g
4:9:10:20
d:hh:mm:ss,0000000
General extended format, G
4:09:20:15,0000000
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.