Events
An
event
occurs at runtime to indicate that a certain situation has occurred. An action or method is then performed. Both users and the system can cause events on the HMI device. For example, an event can occur when the user clicks the mouse button. The system can also trigger events. For example, an event could occur when a graphic element enters a specific state, such as a color changing values.Events include:
- Mouse click
- Mouse down
- Mouse up
- Load project
- Variable value changes
- Variable value meets specified condition
- Variable value is out of specified range
Events perform methods to create application logic. Add a method to an event and configure that method to have the event perform the method at runtime. For each event, you must configure one or more methods to perform. When the event is triggered, the configured method occurs. Methods, dependent on type of event and element, include:
- Create object
- Create variable
- Delete node
- Increment value
- Set bit value
- Set variable value
- Toggle value
- Toggle bit
- Open dialog
- Acknowledge all active alarms
- Confirm all active alarms
- Change user
- Modify text
Provide Feedback