Add an image
Add an image to the canvas to insert an empty image and then specify the image the object is to display. You can change the image that the object displays.
- InProject view, right-click the object or folder to contain the image and then select .
- Double-click the empty image
that appears on the canvas.
TIP: If you resize the image to make it larger, the message
appears.Double click to select a picture - InSelect file, select the image to display and then chooseSelect.TIP:To find items, start typing the item name to find inSelect file.If the file does not appear inSelect file, selectand inImport file(s)Import file(s), select the file to import and then chooseSelect.
image
Provide Feedback