Connect to remote access

Configure remote access to the device as well as remote assistance through the
FactoryTalk Remote Access
Widget.
  1. On the device, open the screen with the FactoryTalk Remote Access Widget.
    If you created your project using the OptixPanel template on the start page, select
    Settings
    and then select
    FT Remote Access
    On the
    Connections
    tab of the widget,
    FT Remote Access runtime version
    displays the version that is running on the device.
  2. To connect the device to the
    FactoryTalk Remote Access
    application, select
    Connections
    .
  3. Under
    FT Remote Access connection
    , select
    Connect
    .
    If your device is already added to the
    FactoryTalk Remote Access
    domain, the device is automatically connected. If your device is not in the
    FactoryTalk Remote Access
    domain, you are prompted to add your device in FactoryTalk Remote Access with the displayed device id and password. 
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.