Add optional objects to a node
Add optional objects to the objects that support them.
TIP:
The available optional objects depend on the type definition of the parent object.
Prerequisites
Add nodes to the project. See Add instances of types defined in Companion Specifications.
- To add optional objects to a node
- Right-click an object and select.
The optional object appears under the node.
Provide Feedback