Create a NetLogic that fetches UI
Create a NetLogic that fetches UI elements from the OPC UA server.
Set the default external code editor. See Set the default code editor.
- To create a NetLogic that fetches UI
- InProject view, right-clickMainWindow (type)and select .
- Hover-over the NetLogic, select, and enterUIFetcher.
- Double-click the NetLogic.The external code editor opens.
- In the code editor, replace the existing code with the following code:#region StandardUsing using System; using FTOptix.Core; using FTOptix.CoreBase; using FTOptix.HMIProject; using UAManagedCore; using OpcUa = UAManagedCore.OpcUa; using FTOptix.NetLogic; using FTOptix.UI; using FTOptix.OPCUAServer; #endregion public class UIFetcher : FTOptix.NetLogic.BaseNetLogic { public override void Start() { myDelayedTask = new DelayedTask(LoadRemotePanel, 2000, LogicObject); myDelayedTask.Start(); } public void LoadRemotePanel() { var clientPanelLoader = (PanelLoader)LogicObject.Owner.Get("ClientPanelLoader"); var remoteMainPanel = Project.Current.Get("UI/RemotePanels/MainPanel"); if (remoteMainPanel == null) { Log.Error("Remote server main panel not found"); return; } clientPanelLoader.ChangePanel(remoteMainPanel.NodeId, NodeId.Empty); } [ExportMethod] public void ReloadRemote() { Start(); } public override void Stop() { // Insert code to be executed when the user-defined logic is stopped myDelayedTask.Dispose(); } private DelayedTask myDelayedTask; }
- Save the code.
Provide Feedback