Import nodes from NodeSet

Import all nodes from a NodeSet
XML
file.
TIP: Import nodes from NodeSet to import all nodes from
OPC UA Companion Specifications
defined in a NodeSet file. For more information, see OPC UA Companion Specifications.
Prerequisites
Obtain an
XML
file with NodeSet to import.
  1. To import nodes from NodeSet
  2. In
    Project view
    , right-click
    Model
    folder or any of its subfolders and then select
    New
    Import from NodeSet
    .
  3. Select the
    XML
    with NodeSet to import.
The imported nodes appear in the folder. If you import the nodes into the same location again, all changes to the already imported nodes are retained.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.