Add a range to a variable
Add minimum and maximum limits to numeric variables. Limits impose certain behaviors when the value is outside of the limits.
- InProject view, select a variable.
- InProperties, right-click the numerical variable name and select .
- UnderEURange, complete:
- Low limit. The low limit of the variable value
- High limit. The upper limit of the variable value.
- Constrain. IfTrue, constrains the values for the variable to the low and high limits.
range
Provide Feedback