Network interfaces variables

Bind a property of graphic object to a predefined
Network interfaces
variable in the
Additional IP addresses
object to configure the network for your HMI device. For example, bind to the
IP addresses
variable to specify the IP address for the HMI device. To bind to a variable, see Create dynamic links.
The
Additional IP addresses
category under
Network interfaces
in the Dynamic Link browser displays the variables related to the HMI device.
Additional IP addresses variables
Variable
Type
Definition
Read or Write
Reboot Required
Interface name
String
Name of the interface
Read-only
Reboot not required
DHCP activated
Boolean
Obtain IP settings automatically using DHCP
Read/Write
Reboot required
IP address
String
IP address of the network
Read/Write
Reboot required
Mask
String
Subnet mask of the network
Read/Write
Reboot required
DNS 1
String
Primary DNS address of the network
Read/Write
Reboot required
DNS 2
String
Secondary DNS address of the network
Read/Write
Reboot required
Default gateway
String
IP address of the default network gateway
Read/Write
Reboot required
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.