Restore a previous version of a project
Restore a previous version of a local or remote project.
When you restore a commit, the project on your local computer updates to include the contents of the selected commit. Restoring a commit permanently deletes any commits that occurred after the restored commit. Restore a commit from
Version history
.- In the main toolbar of the open project, select.View history
- Selectto select the commit and the version of the project to restore.
- SelectRestore.
Version history
closes and the open project includes the changes of the selected commit.restore project
Provide Feedback