Export a FactoryTalk Optix Application
Export a
FactoryTalk Optix Application
to deploy the application to target devices that are not accessible in the network.- Select the arrow next toto open the drop-down menu and then select .Save
- In the dialog, complete:
- Platform. Select the operating system of the target device.
- Location. Type the path to the location where you want to save theFactoryTalk Optix Application. Alternatively, select the folder icon to browse to the folder.TIP: A folder can only contain oneFactoryTalk Optix Application. EachFactoryTalk Optix Applicationmust use a separate folder.
- (optional) If available, fillPasswordto password-protect the exported application.The exported application is encrypted. You will be prompted to enter the password when importing the application to the target device.
- SelectExport.
A progress window displays while the
FactoryTalk Optix Application
is being exported. After the export has completed, a dialog appears to inform you that the FactoryTalk Optix Application
was successfully exported to the location specified.export
Provide Feedback