Select a client device
Select an already configured client device to deploy
FactoryTalk Optix Applications
over the network to the client device.- From the main toolbar, next toRun
- (optional) InClient device settings, to display only the active remote client devices, toggleActive remote devices.TIP: Refresh remote client devices by selectingRefresh.
- Select a client device.
- ChooseSelect.
Provide Feedback