Search
FactoryTalk Optix Help
NetLogics management
Create, modify, and execute NetLogic to extend your project with custom logic. Use an external editor to edit the code of a NetLogic.
To manage NetLogics:
Set the default code editor
Create a NetLogic
Edit a NetLogic
Run a NetLogic at design time
Open the project in an external code editor
NetLogic
Set the default code editor
Create a NetLogic
Edit a NetLogic
Run a NetLogic at design time
Open the project in an external code editor
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.