Information model
The information model organizes nodes in projects. The main project node is the root node.
TIP:
A node is any object, object type, variable, variable type, custom data type, or method in the project.
NOTE:
See Terms dictionary to learn more about node and information model.
Node information model
The node information model indicates the set of nodes that describes the structure and characteristics of the node.
For example, a Motor object may consist of a Stator object and a Crankshaft object. Each of these objects can contain variables that describe their properties.
Project information model
The project information model is the information model of the root project node that includes every object, object type, variable, variable type, custom data type, or method in the project.
The name of the root node is the name of the project. The nodes may be organized into folders.
The structure of the project can mirror the physical structure of machines.
TIP:
Structuring modular machines in an application as they appear in the physical environment makes it easier to manage them in the project.
Provide Feedback