Create MotorPanel instances

Instantiate the MotorPanel type and create the required dynamic links.
  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    MotorPanel
    twice.
    Under
    MainWindow (type)
    ,
    MotorPanel1
    and
    MotorPanel2
    appear.
  2. Select
    MotorPanel1
    and in
    Properties
    , create a dynamic link between
    MotorAlias
    and
    ProjectName
    Model
    Motor1
    .
    For more information about dynamic links, see Create dynamic links.
  3. Select
    MotorPanel2
    and in
    Properties
    , create a dynamic link between
    MotorAlias
    and
    ProjectName
    Model
    Motor2
    .
    For more information about dynamic links, see Create dynamic links.
Based on the
MotorAlias
values, the
MotorExt
values are set automatically.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.